Part Number: DS90UB913A-CXEVM
The DS90UB913A eval board has jumpers for 3.3V and 1.8V selection.
Which way should the jumpers be if I want to provide 1.8V input on the serializer JP1 pins? Please provide guidance on setting JP13 and JP8 since the user manual is not clear (just says "selects 3.3" or "selects 1.8"...) Should I put JP13 on the 0V side for 1.8V input? Or leave the jumper off completely?
Last question: can I provide 1.8V input to the serializer, with 3.3V output on the deserializer, and power over coax with 5V at the DEserializer?