Other Parts Discussed in Thread: TPS25740A
I'm designing a USB type-C device for a customer that connects to an Android phone. The solution needs to charge the phone as well as appear to the phone as a USB 2.0 device (USB-serial converter). The phone only supports charging at 5V, 2A and 9V, 2A. I'm new to USB type-C but as far as I understand it, this can be accomplished by selecting a CC and PD controller that can send the PR_Swap or DR_Swap commands to negotiate this behavior.
I have a TPS65986EMV evaluation board that I've been testing out but the challenge I'm running into is the fact that the high voltage mode on the eval module doesn't work with any voltage lower than 12V. My question is this: is it possible to do what I need to do with a single chip, or do I need to implement a 9V source with something like a TPS25740A and a hub, like the TIDA-00630 reference design (without the DisplayPort features)?