Hello,
In the AC electrical characteristics table, Note 6 implies 3 parts in parallel (8.2 NH, 0.5 pF, and 75 ohms) on the SD344 evaluation board.
The typical application Figure 3 drawings shows just a 3.9 nH in parallel with the 75 ohms.
The layout example appears to show 5 parts on the input (2 in parallel, 2 in series to GND, and then the 1.0 uF cap to the input)
The different sections of the datasheet appear to contradict.
Can you supply the SD344 eval board schematics and layout to clarify?
Thanks,
Jordan