This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65MLVD200A: Max voltage on pin A/B

Part Number: SN65MLVD200A
Other Parts Discussed in Thread: SN65MLVD202A

Hi team,

My customer is using SN65MLVD200A, and they found that in their system bus, the chip's A/B pin will connect 5V power supply with a 4.7kohm pull-up resistor.

In datasheet, the max condition is 4V for A/B pin. But since it's only a weak pull-up, could the chip work normally in such condition?

If RE/DE pin is set to make the chip disabled, could it help the chip survive in such condition?

Thank you!