The TI E2E™ design support forums will undergo maintenance from Sept. 28 to Oct. 2. If you need design support during this time, contact your TI representative or open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDT41: SN65LVDT14

Part Number: SN65LVDT41
Other Parts Discussed in Thread: SN65LVDT14, DRV8860

Regarding the VIH levels for the D or R inputs of the SN65LVDT14 and SN65LVDT41, can I assume that these inputs can safely tolerate 5.7V? The reason I ask is that I plan to drive these inputs with the Dout of a DRV8860 (also a TI device) and this Dout is internally pulled to 5.7V in the DRV8860. The absolute maximum is 6V but there is no maximum voltage for VIH in the Recommended Operating Conditions.

Regards,

James