Hello,
I am using TPS 2052BDR at USB section for load current limit.
Measured following conditions:
Load enabled before boot up - During this condition TPS 2052 is taking current load of 1A and at 1.1A it is going to short circuit mode.
Load enabled after boot up - During this condition TPS 2052 is taking current load of 1.5A and at 1.6A it is going to short circuit mode.
The datasheet shows, each port load current limit is 500mA, but the device is taking more than 500mA.
Please, check and let us know the current limit values.
Regards,
Harish.