Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDT388A: Missing Termination Resistor in IBIS Model

Genius 4535 points
Part Number: SN65LVDT388A

Hi,

In the IBIS model of the SN65LVDT388A device the termination resistors are missing. I'm aware of this post: e2e.ti.com/.../1460464

Because the simulation software extract the model out of the schematic I would like to include the termination resistors in the IBIS model rather than include the resistors in the schematic.
I would do the implementation of this resistors in the IBIS model as follows (showing the first input pin pairs):

[Series Pin Mapping] pin_2    model_name     function_table_group
|
1          2       diff_term_110
3          4       diff_term_110
|
|************************************************************************
|                       110 Ohm differential terminator
|************************************************************************
|
[Model]          diff_term_110
Model_type       Series
|                         (typ)               (min)               (max)
|
C_comp                    0.0000pF            0.0000pF            0.0000pF
[Temperature Range]       25.0                85.0                -40.0
[Voltage Range]           3.3V                3.0V                3.6V
[R Series]                110                 132                 88

I'm unshure about the values of [Temperature Range], [Voltage Range] and [R Series].
Can a TI IBIS expert have a look on those values?

Thanks and best regards,
Patrick