Hi Team,
I am considering using the TDP1E10B09-Q1 in an automotive application where it is protecting lines that go off board. This means those lines are susceptible to a short to battery condition up to 18V. I noticed the breakdown voltage is 9V.. What will happen to the device if the lines it is protecting are shorted to battery at 18V? Will the device be damaged if the short happens for an extended period of time?
Please let me know if this device is acceptable in that type of application.
Thank you!
Jared