Part Number: DS30EA101
Other Parts Discussed in Thread: DS15EA101,
Hi team,
Since the data rate the customer want to use this time is 1.2 Gbps,
I thought DS15EA101 for 1.5 Gbps was reasonable as an equalizer,
Because I did not have an evaluation kit, I purchased DS30EA101 for 3.0 Gbps.
However, when evaluated, DS30EA101 seemed to be slightly unsatisfactory in characteristics.
So there is a question, but when using at 1.2 Gbps,
Is there anything that the DS15EA101 can handle a larger transmission path loss (the equalizer's capability at 1.2 Gbps is higher)?
Is it possible to replace DS15EA101 with the DS30EA101 evaluation kit land pattern?
Thanks
BR
Shidara