Part Number: DS26LV32AT
I'm using the DS26LV32AT Quad Differential Line Receiver and want the Open Input failsafe to result in a low state when the receiver inputs are open or idle. Can an external bias in a power termination configuration be applied to the receiver input with the inverting input pulled up to Vcc and the non-inverting input pulled down to Gnd? The setup would be similar to Figure 9 of AN-903 (below) with Vcc and Gnd swapped.