Hi, Team
I am using the DS90UB903 & DS90UB904 Serdes pair to transfer image, and I have a trouble:
the register 0x0C's field LINK DETECT of 903 is 1 when not connected with the 904(the cable is plug out), even when no valid input pclk detected(the PCLK DETECT is 0).
according to the datasheet, the LINK DETECT = 1 means that the 903 has detected the presence of the 904. May be the datasheet is wrong?
Or the IC we bought is fake??
Thank you
Best Regards