This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A-CXEVM: Using TI913 Serializer to generate Test Image Patterns

Part Number: DS90UB913A-CXEVM
Other Parts Discussed in Thread: DS90UB953-Q1EVM, , DS90UB913A-Q1

Hi,


We design a tester to test board with 8 ports CAMs using 8 [DS90UB953-Q1EVM]. And we were able to test 6 of the ports. Then we informed that the other two ports need different format and they accept TI913 Serializer format.

Q1) Can we use the DS90UB913A-CXEVM Serializer to generate image patterns similar to the TI953? Any information about setting the pattern generator registers/ Hardware setup?

Q2) is there any spatial pattern image format can be generated using TI913 and cannot be generated by TI953?

The information I have about the required image:


• Simulate 1M camera:
• BT.601 or BT.656, DVP protocol (8 bit)
• Upper 8 bits are used, External H-Sync and V-Sync signal lines
• YUV422 (YCbCr)

Thank you,

Aziz,