Dear *,
i have some questions regarding TVS protection
1) When do we have to chose or look at 8/20 waveform and when 10/1000 waveform, how do i know if i need 8/20 protection device or 10/1000 protection device?
2) Why do i choose TVS0500 over traditional TVS diode, what are the benefits?
3) is the steeper i/V of TVS0500 regarding to traditional TVS better and why?
4) What does mean this in ds?
a)
Robust Surge Protection: – IEC61000-4-5 (8/20 µs): 43 A – IEC61643-321 (10/1000 µs): 22 A
b)
Integrated Level 4 IEC 61000-4-2 ESD Protection
Best Regards,
D.