This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867CR: As for Peripheral device of DP83867CRRGZT

Part Number: DP83867CR

Our Customer ask us the following question, and could you kindly answer them?

A) Is there any problem that DP83867CRRGZT and HX5008NL, Pulse Electronics Networking are used together?

B) Could you tell me the recomended pulse trans or RJ45 connector with pulse trans, when DP83867CRRGZT is used?

Thank you & Best Regards,

  • Hi Kiroku-san,

    The HX5008NL should work with the DP83867CR. I have not heard of any issues with this magnetic paired with the PHY.
    We do not have a recommended list since there are so many on the market.
    Please ensure that the magnetic is IEEE 802.3 certified and that the center taps are not shorted together.
    Each center tap must be separate and have its own 0.1uF decoupling cap to ground.
  • Dear Ross san,


    Thank you for your prompt reply.

    I answered your reply to our costomer. If additional inquiry caused, I will contact you.

    Thank you & Best Regards,