This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD101: I have two Sensors Output coming from Tiva C Series controller. May i know how to connect this two Outputs to the TIOL111.

Part Number: SN65HVD101
Other Parts Discussed in Thread: TIOL111, TIOS101

Hello,

    As in Datasheet only one Output goes from controller to TIOL111 IO link as input but in My case I have two Outputs can anyone give some  idea how to interface?

   In Pinout configuration of TIOL111 only one Tx pin is there. If suppose two Outputs is connected to one Tx pin, how the Data Transmission occurs?

   Please share your opinions.

Thank you    

  • Venkatesh,

    It depends on what you want for your system. Do you want both sensor values communicated independently to a master? If so you may want to use two TIOL111 devices (or one TIOL111 plus one TIOS101). If you are trying to consolidate both sensor values to a single system output, you might consider if some AND or OR logic makes sense for your application.

    Regards,
    Max