This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964-Q1: DS90UB964 line len change interupt detected

Part Number: DS90UB964-Q1


Hello Team

My customer is using DS90UB964 and DS90UB933 to do SRV. Now they have an issue.

When their system running will have following error detect. And the error alsway hanpenen. But the other status is normal.

[root@TSH-DEMO /home/root]# 
[root@TSH-DEMO /home/root]# 
[root@TSH-DEMO /home/root]# dmesg 
[ 1378.524849] ===>in ds901b964_irq_handler() IRQ handler
[ 1378.535979] ===>in showTI964Status(): STS=0x92
[ 1378.535995] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1378.536003] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1378.536011] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1378.536018] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1378.536023] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1378.536028] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1378.536032] in showTI964Status() # IS_RX1 DETECTED 
[ 1378.536037] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1378.536042] in showTI964Status() 0: # PORT_PASS=1 
[ 1378.536046] in showTI964Status() 0: # LOCK_STS=1 
[ 1378.536051] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1378.536056] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1378.536061] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1378.536065] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1378.536070] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1378.536074] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1378.536079] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1378.536083] in showTI964Status() 1: # PORT_PASS=1 
[ 1378.536087] in showTI964Status() 1: # LOCK_STS=1 
[ 1378.536094] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1378.536098] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1378.536102] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1378.536107] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1378.536111] in showTI964Status() 2: # PORT_PASS=1 
[ 1378.536115] in showTI964Status() 2: # LOCK_STS=1 
[ 1378.536119] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1378.536124] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1378.536128] in showTI964Status() 3: # PORT_PASS=1 
[ 1378.536132] in showTI964Status() 3: # LOCK_STS=1 
[ 1378.536136] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1378.536143] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1378.536148] ===>in ds901b964_work_func() need reset? YES!!!
[ 1378.552623] in mxc_ipu_channel_reset() start
[ 1378.702650] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1378.702690] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1378.702730] in mxc_ipu_channel_reset() end
[ 1378.735574] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1378.767716] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1378.808606] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1378.849516] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1382.184043] ===>in ds901b964_irq_handler() IRQ handler
[ 1382.194868] ===>in showTI964Status(): STS=0x92
[ 1382.194879] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1382.194888] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1382.194895] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1382.194903] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1382.194907] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1382.194914] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1382.194919] in showTI964Status() # IS_RX1 DETECTED 
[ 1382.194925] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1382.194929] in showTI964Status() 0: # PORT_PASS=1 
[ 1382.194934] in showTI964Status() 0: # LOCK_STS=1 
[ 1382.194939] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1382.194945] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1382.194949] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1382.194954] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1382.194959] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1382.194964] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1382.194968] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1382.194972] in showTI964Status() 1: # PORT_PASS=1 
[ 1382.194977] in showTI964Status() 1: # LOCK_STS=1 
[ 1382.194981] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1382.194985] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1382.194989] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1382.194994] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1382.194998] in showTI964Status() 2: # PORT_PASS=1 
[ 1382.195002] in showTI964Status() 2: # LOCK_STS=1 
[ 1382.195006] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1382.195011] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1382.195015] in showTI964Status() 3: # PORT_PASS=1 
[ 1382.195019] in showTI964Status() 3: # LOCK_STS=1 
[ 1382.195023] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1382.195030] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1382.195035] ===>in ds901b964_work_func() need reset? YES!!!
[ 1382.212597] in mxc_ipu_channel_reset() start
[ 1382.302653] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1382.302695] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1382.302808] in mxc_ipu_channel_reset() end
[ 1382.366384] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1382.407272] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1382.448169] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1385.256042] ===>in ds901b964_irq_handler() IRQ handler
[ 1385.266995] ===>in showTI964Status(): STS=0x92
[ 1385.267006] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1385.267015] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1385.267024] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1385.267031] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1385.267036] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1385.267041] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1385.267046] in showTI964Status() # IS_RX1 DETECTED 
[ 1385.267051] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1385.267056] in showTI964Status() 0: # PORT_PASS=1 
[ 1385.267060] in showTI964Status() 0: # LOCK_STS=1 
[ 1385.267065] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1385.267071] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1385.267075] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1385.267080] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1385.267084] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1385.267090] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1385.267095] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1385.267099] in showTI964Status() 1: # PORT_PASS=1 
[ 1385.267103] in showTI964Status() 1: # LOCK_STS=1 
[ 1385.267107] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1385.267112] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1385.267116] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1385.267120] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1385.267125] in showTI964Status() 2: # PORT_PASS=1 
[ 1385.267129] in showTI964Status() 2: # LOCK_STS=1 
[ 1385.267134] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1385.267139] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1385.267143] in showTI964Status() 3: # PORT_PASS=1 
[ 1385.267148] in showTI964Status() 3: # LOCK_STS=1 
[ 1385.267152] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1385.267160] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1385.267164] ===>in ds901b964_work_func() need reset? YES!!!
[ 1385.282601] in mxc_ipu_channel_reset() start
[ 1385.412671] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1385.412712] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1385.412827] in mxc_ipu_channel_reset() end
[ 1385.442167] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1385.474321] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1385.515189] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1385.556101] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1389.540601] ===>in ds901b964_irq_handler() IRQ handler
[ 1389.551642] ===>in showTI964Status(): STS=0x92
[ 1389.551656] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1389.551665] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1389.551673] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1389.551680] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1389.551688] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1389.551694] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1389.551698] in showTI964Status() # IS_RX1 DETECTED 
[ 1389.551704] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1389.551709] in showTI964Status() 0: # PORT_PASS=1 
[ 1389.551714] in showTI964Status() 0: # LOCK_STS=1 
[ 1389.551719] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1389.551725] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1389.551730] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1389.551734] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1389.551739] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1389.551744] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1389.551749] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1389.551753] in showTI964Status() 1: # PORT_PASS=1 
[ 1389.551758] in showTI964Status() 1: # LOCK_STS=1 
[ 1389.551762] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1389.551767] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1389.551771] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1389.551776] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1389.551780] in showTI964Status() 2: # PORT_PASS=1 
[ 1389.551784] in showTI964Status() 2: # LOCK_STS=1 
[ 1389.551788] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1389.551793] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1389.551797] in showTI964Status() 3: # PORT_PASS=1 
[ 1389.551801] in showTI964Status() 3: # LOCK_STS=1 
[ 1389.551806] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1389.551813] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1389.551818] ===>in ds901b964_work_func() need reset? YES!!!
[ 1389.562601] in mxc_ipu_channel_reset() start
[ 1389.702648] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1389.702672] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1389.702732] in mxc_ipu_channel_reset() end
[ 1389.736019] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1389.768150] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1389.809046] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1389.849949] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1391.883004] ===>in ds901b964_irq_handler() IRQ handler
[ 1391.893947] ===>in showTI964Status(): STS=0x92
[ 1391.893958] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1391.893967] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1391.893974] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1391.893981] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1391.893987] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1391.893992] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1391.893996] in showTI964Status() # IS_RX1 DETECTED 
[ 1391.894002] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1391.894007] in showTI964Status() 0: # PORT_PASS=1 
[ 1391.894012] in showTI964Status() 0: # LOCK_STS=1 
[ 1391.894017] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1391.894022] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1391.894027] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1391.894031] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1391.894036] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1391.894041] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1391.894047] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1391.894051] in showTI964Status() 1: # PORT_PASS=1 
[ 1391.894077] in showTI964Status() 1: # LOCK_STS=1 
[ 1391.894083] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1391.894088] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1391.894092] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1391.894097] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1391.894101] in showTI964Status() 2: # PORT_PASS=1 
[ 1391.894105] in showTI964Status() 2: # LOCK_STS=1 
[ 1391.894109] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1391.894114] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1391.894118] in showTI964Status() 3: # PORT_PASS=1 
[ 1391.894122] in showTI964Status() 3: # LOCK_STS=1 
[ 1391.894126] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1391.894133] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1391.894139] ===>in ds901b964_work_func() need reset? YES!!!
[ 1391.912586] in mxc_ipu_channel_reset() start
[ 1392.032640] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1392.032685] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1392.032770] in mxc_ipu_channel_reset() end
[ 1392.066944] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1392.066959] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1392.066987] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1392.099090] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1392.139992] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1392.180886] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1396.469470] ===>in ds901b964_irq_handler() IRQ handler
[ 1396.480578] ===>in showTI964Status(): STS=0x92
[ 1396.480590] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1396.480599] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1396.480634] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1396.480643] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1396.480649] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1396.480656] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1396.480661] in showTI964Status() # IS_RX1 DETECTED 
[ 1396.480668] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1396.480673] in showTI964Status() 0: # PORT_PASS=1 
[ 1396.480678] in showTI964Status() 0: # LOCK_STS=1 
[ 1396.480684] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1396.480689] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1396.480695] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1396.480699] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1396.480705] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1396.480710] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1396.480715] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1396.480720] in showTI964Status() 1: # PORT_PASS=1 
[ 1396.480726] in showTI964Status() 1: # LOCK_STS=1 
[ 1396.480730] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1396.480734] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1396.480738] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1396.480749] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1396.480753] in showTI964Status() 2: # PORT_PASS=1 
[ 1396.480758] in showTI964Status() 2: # LOCK_STS=1 
[ 1396.480762] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1396.480767] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1396.480772] in showTI964Status() 3: # PORT_PASS=1 
[ 1396.480776] in showTI964Status() 3: # LOCK_STS=1 
[ 1396.480780] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1396.480787] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1396.480793] ===>in ds901b964_work_func() need reset? YES!!!
[ 1396.492598] in mxc_ipu_channel_reset() start
[ 1396.612654] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1396.612700] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1396.612782] in mxc_ipu_channel_reset() end
[ 1396.647041] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1396.647060] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1396.647072] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1396.647088] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1396.679191] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1396.720087] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1396.760993] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1397.442753] ===>in ds901b964_irq_handler() IRQ handler
[ 1397.454570] ===>in showTI964Status(): STS=0x92
[ 1397.454581] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1397.454590] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1397.454597] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1397.454605] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1397.454611] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1397.454615] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1397.454620] in showTI964Status() # IS_RX1 DETECTED 
[ 1397.454626] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1397.454631] in showTI964Status() 0: # PORT_PASS=1 
[ 1397.454635] in showTI964Status() 0: # LOCK_STS=1 
[ 1397.454640] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1397.454644] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1397.454649] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1397.454653] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1397.454658] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1397.454662] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1397.454667] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1397.454671] in showTI964Status() 1: # PORT_PASS=1 
[ 1397.454675] in showTI964Status() 1: # LOCK_STS=1 
[ 1397.454679] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1397.454683] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1397.454688] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1397.454692] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1397.454696] in showTI964Status() 2: # PORT_PASS=1 
[ 1397.454700] in showTI964Status() 2: # LOCK_STS=1 
[ 1397.454704] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1397.454709] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1397.454713] in showTI964Status() 3: # PORT_PASS=1 
[ 1397.454717] in showTI964Status() 3: # LOCK_STS=1 
[ 1397.454722] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1397.454730] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1397.454735] ===>in ds901b964_work_func() need reset? YES!!!
[ 1397.472589] in mxc_ipu_channel_reset() start
[ 1397.592632] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1397.592676] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1397.592796] in mxc_ipu_channel_reset() end
[ 1397.628493] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1397.628508] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1397.628528] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1397.660641] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1397.701575] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1397.742432] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1401.326701] ===>in ds901b964_irq_handler() IRQ handler
[ 1401.337363] ===>in showTI964Status(): STS=0x92
[ 1401.337374] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1401.337382] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1401.337390] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1401.337398] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1401.337404] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1401.337409] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1401.337413] in showTI964Status() # IS_RX1 DETECTED 
[ 1401.337418] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1401.337423] in showTI964Status() 0: # PORT_PASS=1 
[ 1401.337427] in showTI964Status() 0: # LOCK_STS=1 
[ 1401.337433] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1401.337440] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1401.337445] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1401.337449] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1401.337454] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1401.337459] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1401.337463] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1401.337467] in showTI964Status() 1: # PORT_PASS=1 
[ 1401.337471] in showTI964Status() 1: # LOCK_STS=1 
[ 1401.337476] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1401.337480] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1401.337484] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1401.337489] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1401.337493] in showTI964Status() 2: # PORT_PASS=1 
[ 1401.337497] in showTI964Status() 2: # LOCK_STS=1 
[ 1401.337502] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1401.337506] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1401.337510] in showTI964Status() 3: # PORT_PASS=1 
[ 1401.337514] in showTI964Status() 3: # LOCK_STS=1 
[ 1401.337519] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1401.337526] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1401.337532] ===>in ds901b964_work_func() need reset? YES!!!
[ 1401.352596] in mxc_ipu_channel_reset() start
[ 1401.482646] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1401.482719] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1401.482805] in mxc_ipu_channel_reset() end
[ 1401.513398] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1401.513426] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1401.513439] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1401.513455] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1401.545558] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1401.586446] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1401.627350] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1402.978673] ===>in ds901b964_irq_handler() IRQ handler
[ 1402.990295] ===>in showTI964Status(): STS=0x92
[ 1402.990317] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1402.990326] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1402.990333] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1402.990340] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1402.990346] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1402.990351] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1402.990356] in showTI964Status() # IS_RX1 DETECTED 
[ 1402.990361] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1402.990366] in showTI964Status() 0: # PORT_PASS=1 
[ 1402.990371] in showTI964Status() 0: # LOCK_STS=1 
[ 1402.990376] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1402.990381] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1402.990385] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1402.990390] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1402.990395] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1402.990399] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1402.990404] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1402.990408] in showTI964Status() 1: # PORT_PASS=1 
[ 1402.990412] in showTI964Status() 1: # LOCK_STS=1 
[ 1402.990417] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1402.990421] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1402.990425] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1402.990430] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1402.990434] in showTI964Status() 2: # PORT_PASS=1 
[ 1402.990438] in showTI964Status() 2: # LOCK_STS=1 
[ 1402.990442] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1402.990447] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1402.990451] in showTI964Status() 3: # PORT_PASS=1 
[ 1402.990455] in showTI964Status() 3: # LOCK_STS=1 
[ 1402.990459] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1402.990467] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1402.990471] ===>in ds901b964_work_func() need reset? YES!!!
[ 1403.002627] in mxc_ipu_channel_reset() start
[ 1403.152644] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1403.152690] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1403.152771] in mxc_ipu_channel_reset() end
[ 1403.190046] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1403.190066] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1403.190084] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1403.222199] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1403.263100] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1403.304009] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1408.993692] ===>in ds901b964_irq_handler() IRQ handler
[ 1409.006939] ===>in showTI964Status(): STS=0x92
[ 1409.006956] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1409.006965] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1409.006973] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1409.006980] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1409.007012] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1409.007018] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1409.007024] in showTI964Status() # IS_RX1 DETECTED 
[ 1409.007030] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1409.007035] in showTI964Status() 0: # PORT_PASS=1 
[ 1409.007040] in showTI964Status() 0: # LOCK_STS=1 
[ 1409.007045] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1409.007051] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1409.007057] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1409.007061] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1409.007066] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1409.007071] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1409.007075] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1409.007080] in showTI964Status() 1: # PORT_PASS=1 
[ 1409.007084] in showTI964Status() 1: # LOCK_STS=1 
[ 1409.007089] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1409.007093] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1409.007098] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1409.007102] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1409.007106] in showTI964Status() 2: # PORT_PASS=1 
[ 1409.007110] in showTI964Status() 2: # LOCK_STS=1 
[ 1409.007115] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1409.007119] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1409.007123] in showTI964Status() 3: # PORT_PASS=1 
[ 1409.007128] in showTI964Status() 3: # LOCK_STS=1 
[ 1409.007132] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1409.007139] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1409.007144] ===>in ds901b964_work_func() need reset? YES!!!
[ 1409.022589] in mxc_ipu_channel_reset() start
[ 1409.162636] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1409.162681] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1409.162767] in mxc_ipu_channel_reset() end
[ 1409.201429] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1409.201459] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1409.201476] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1409.233597] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1409.274485] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1409.315369] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1416.136720] ===>in ds901b964_irq_handler() IRQ handler
[ 1416.147188] ===>in showTI964Status(): STS=0x92
[ 1416.147200] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1416.147209] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1416.147218] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1416.147226] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1416.147232] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1416.147239] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1416.147244] in showTI964Status() # IS_RX1 DETECTED 
[ 1416.147256] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1416.147261] in showTI964Status() 0: # PORT_PASS=1 
[ 1416.147266] in showTI964Status() 0: # LOCK_STS=1 
[ 1416.147271] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1416.147277] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1416.147282] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1416.147287] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1416.147292] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1416.147297] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1416.147302] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1416.147306] in showTI964Status() 1: # PORT_PASS=1 
[ 1416.147310] in showTI964Status() 1: # LOCK_STS=1 
[ 1416.147316] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1416.147320] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1416.147324] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1416.147331] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1416.147336] in showTI964Status() 2: # PORT_PASS=1 
[ 1416.147341] in showTI964Status() 2: # LOCK_STS=1 
[ 1416.147346] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1416.147352] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1416.147357] in showTI964Status() 3: # PORT_PASS=1 
[ 1416.147362] in showTI964Status() 3: # LOCK_STS=1 
[ 1416.147367] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1416.147375] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1416.147381] ===>in ds901b964_work_func() need reset? YES!!!
[ 1416.162587] in mxc_ipu_channel_reset() start
[ 1416.282643] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1416.282693] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1416.282780] in mxc_ipu_channel_reset() end
[ 1416.316946] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1416.316976] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1416.316988] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1416.317004] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1416.349120] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1416.389988] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1416.430890] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1422.341283] ===>in ds901b964_irq_handler() IRQ handler
[ 1422.352598] ===>in showTI964Status(): STS=0x92
[ 1422.352609] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1422.352618] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1422.352625] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1422.352633] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1422.352638] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1422.352643] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1422.352647] in showTI964Status() # IS_RX1 DETECTED 
[ 1422.352652] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1422.352657] in showTI964Status() 0: # PORT_PASS=1 
[ 1422.352661] in showTI964Status() 0: # LOCK_STS=1 
[ 1422.352667] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1422.352671] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1422.352676] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1422.352681] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1422.352685] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1422.352690] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1422.352696] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1422.352700] in showTI964Status() 1: # PORT_PASS=1 
[ 1422.352704] in showTI964Status() 1: # LOCK_STS=1 
[ 1422.352708] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1422.352712] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1422.352717] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1422.352721] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1422.352725] in showTI964Status() 2: # PORT_PASS=1 
[ 1422.352729] in showTI964Status() 2: # LOCK_STS=1 
[ 1422.352733] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1422.352738] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1422.352742] in showTI964Status() 3: # PORT_PASS=1 
[ 1422.352746] in showTI964Status() 3: # LOCK_STS=1 
[ 1422.352750] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1422.352757] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1422.352762] ===>in ds901b964_work_func() need reset? YES!!!
[ 1422.372594] in mxc_ipu_channel_reset() start
[ 1422.502681] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1422.502725] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1422.502809] in mxc_ipu_channel_reset() end
[ 1422.532821] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1422.532850] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1422.532862] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1422.532878] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1422.564989] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1422.605852] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1422.646786] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1423.034701] ===>in ds901b964_irq_handler() IRQ handler
[ 1423.045557] ===>in showTI964Status(): STS=0x92
[ 1423.045570] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1423.045579] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1423.045586] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1423.045594] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1423.045598] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1423.045604] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1423.045609] in showTI964Status() # IS_RX1 DETECTED 
[ 1423.045614] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1423.045619] in showTI964Status() 0: # PORT_PASS=1 
[ 1423.045623] in showTI964Status() 0: # LOCK_STS=1 
[ 1423.045628] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1423.045633] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1423.045638] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1423.045643] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1423.045647] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1423.045652] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1423.045657] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1423.045661] in showTI964Status() 1: # PORT_PASS=1 
[ 1423.045665] in showTI964Status() 1: # LOCK_STS=1 
[ 1423.045669] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1423.045673] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1423.045678] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1423.045683] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1423.045687] in showTI964Status() 2: # PORT_PASS=1 
[ 1423.045691] in showTI964Status() 2: # LOCK_STS=1 
[ 1423.045696] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1423.045701] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1423.045705] in showTI964Status() 3: # PORT_PASS=1 
[ 1423.045709] in showTI964Status() 3: # LOCK_STS=1 
[ 1423.045714] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1423.045721] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1423.045725] ===>in ds901b964_work_func() need reset? YES!!!
[ 1423.062587] in mxc_ipu_channel_reset() start
[ 1423.192645] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1423.192690] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1423.192775] in mxc_ipu_channel_reset() end
[ 1423.227993] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1423.228008] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1423.228026] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1423.260168] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1423.301056] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1423.341947] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1425.262625] ===>in ds901b964_irq_handler() IRQ handler
[ 1425.273310] ===>in showTI964Status(): STS=0x91
[ 1425.273321] LO[0]=0x03 HI[0]=0x00 ST1[0]=0x13 ST2[0]=0x00
[ 1425.273330] LO[1]=0x60 HI[1]=0x00 ST1[1]=0x43 ST2[1]=0x45
[ 1425.273337] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1425.273345] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1425.273350] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1425.273356] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1425.273361] in showTI964Status() # IS_RX0 DETECTED 
[ 1425.273367] in showTI964Status() 0: # IS_PORT_PASS DETECTED 
[ 1425.273372] in showTI964Status() 0: # IS_LOCK_STS DETECTED 
[ 1425.273377] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1425.273381] in showTI964Status() 0: # LOCK_STS_CHG DETECTED 
[ 1425.273386] in showTI964Status() 0: # PORT_PASS=1 
[ 1425.273391] in showTI964Status() 0: # LOCK_STS=1 
[ 1425.273396] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1425.273401] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1425.273405] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1425.273409] in showTI964Status() 1: # PORT_PASS=1 
[ 1425.273414] in showTI964Status() 1: # LOCK_STS=1 
[ 1425.273418] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1425.273422] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1425.273427] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1425.273431] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1425.273435] in showTI964Status() 2: # PORT_PASS=1 
[ 1425.273439] in showTI964Status() 2: # LOCK_STS=1 
[ 1425.273443] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1425.273448] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1425.273452] in showTI964Status() 3: # PORT_PASS=1 
[ 1425.273456] in showTI964Status() 3: # LOCK_STS=1 
[ 1425.273460] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1425.273467] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1425.273472] ===>in ds901b964_work_func() need reset? YES!!!
[ 1425.292596] in mxc_ipu_channel_reset() start
[ 1425.442643] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1425.442694] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1425.442782] in mxc_ipu_channel_reset() end
[ 1425.477157] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1425.477175] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001
[ 1425.477188] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1425.477206] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1425.509307] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1425.550191] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1425.591106] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1428.346399] ===>in ds901b964_irq_handler() IRQ handler
[ 1428.357255] ===>in showTI964Status(): STS=0x91
[ 1428.357267] LO[0]=0x63 HI[0]=0x00 ST1[0]=0x10 ST2[0]=0x43
[ 1428.357276] LO[1]=0x00 HI[1]=0x00 ST1[1]=0x43 ST2[1]=0x04
[ 1428.357283] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1428.357291] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1428.357296] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1428.357301] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1428.357306] in showTI964Status() # IS_RX0 DETECTED 
[ 1428.357311] in showTI964Status() 0: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1428.357316] in showTI964Status() 0: # IS_LINE_CNT_CHG DETECTED 
[ 1428.357320] in showTI964Status() 0: # IS_PORT_PASS DETECTED 
[ 1428.357325] in showTI964Status() 0: # IS_LOCK_STS DETECTED 
[ 1428.357330] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1428.357335] in showTI964Status() 0: # LOCK_STS_CHG DETECTED 
[ 1428.357340] in showTI964Status() 0: # LINE_LEN_CHG 
[ 1428.357344] in showTI964Status() 0: # NO_FPD3_CLK DETECTED 
[ 1428.357349] in showTI964Status() 0: # LINE_CNT_CHG DETECTED 
[ 1428.357355] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1428.357359] in showTI964Status() 1: # PORT_PASS=1 
[ 1428.357364] in showTI964Status() 1: # LOCK_STS=1 
[ 1428.357368] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1428.357373] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1428.357377] in showTI964Status() 2: # PORT_PASS=1 
[ 1428.357381] in showTI964Status() 2: # LOCK_STS=1 
[ 1428.357385] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1428.357390] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1428.357394] in showTI964Status() 3: # PORT_PASS=1 
[ 1428.357398] in showTI964Status() 3: # LOCK_STS=1 
[ 1428.357402] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1428.357409] ds901b964_work_func old_mask=0x0F new_mask=0x0E sub_mask=0x01 add_mask=0x00
[ 1428.357415] ===>in ds901b964_work_func() need reset? YES!!!
[ 1428.377134] in mxc_ipu_channel_reset() start
[ 1429.002645] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1429.002691] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1429.002776] in mxc_ipu_channel_reset() end
[ 1429.002793] ===>in ds901b964_irq_handler() IRQ handler
[ 1429.013196] ===>in showTI964Status(): STS=0x92
[ 1429.013207] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x00 ST2[0]=0x02
[ 1429.013215] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1429.013222] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1429.013229] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1429.013235] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1429.013241] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1429.013246] in showTI964Status() # IS_RX1 DETECTED 
[ 1429.013252] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1429.013257] in showTI964Status() 0: # NO_FPD3_CLK DETECTED 
[ 1429.013262] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1429.013268] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1429.013272] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1429.013278] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1429.013283] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1429.013289] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1429.013294] in showTI964Status() 1: # PORT_PASS=1 
[ 1429.013299] in showTI964Status() 1: # LOCK_STS=1 
[ 1429.013305] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1429.013309] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1429.013313] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1429.013318] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1429.013322] in showTI964Status() 2: # PORT_PASS=1 
[ 1429.013326] in showTI964Status() 2: # LOCK_STS=1 
[ 1429.013330] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1429.013335] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1429.013339] in showTI964Status() 3: # PORT_PASS=1 
[ 1429.013343] in showTI964Status() 3: # LOCK_STS=1 
[ 1429.013347] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1429.013354] ds901b964_work_func old_mask=0x0E new_mask=0x0E sub_mask=0x00 add_mask=0x00
[ 1429.013360] ===>in ds901b964_work_func() need reset? YES!!!
[ 1429.032591] in mxc_ipu_channel_reset() start
[ 1429.034916] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1429.034936] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1429.372602] xd_mipi: mxc_v4l_dqueue timeout enc_counter 1
[ 1429.639513] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1429.639555] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1429.639635] in mxc_ipu_channel_reset() end
[ 1429.648328] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1429.648348] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1429.648365] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1429.685641] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1429.726526] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1429.767439] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1432.710930] ===>in ds901b964_irq_handler() IRQ handler
[ 1432.722402] ===>in showTI964Status(): STS=0x92
[ 1432.722419] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x00 ST2[0]=0x02
[ 1432.722428] LO[1]=0x03 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x04
[ 1432.722435] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1432.722443] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1432.722449] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1432.722454] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1432.722458] in showTI964Status() # IS_RX1 DETECTED 
[ 1432.722465] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1432.722469] in showTI964Status() 0: # NO_FPD3_CLK DETECTED 
[ 1432.722474] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1432.722479] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1432.722484] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1432.722489] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1432.722493] in showTI964Status() 1: # PORT_PASS=1 
[ 1432.722497] in showTI964Status() 1: # LOCK_STS=1 
[ 1432.722502] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1432.722507] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1432.722511] in showTI964Status() 2: # PORT_PASS=1 
[ 1432.722515] in showTI964Status() 2: # LOCK_STS=1 
[ 1432.722519] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1432.722524] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1432.722528] in showTI964Status() 3: # PORT_PASS=1 
[ 1432.722532] in showTI964Status() 3: # LOCK_STS=1 
[ 1432.722536] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1432.722543] ds901b964_work_func old_mask=0x0E new_mask=0x0E sub_mask=0x00 add_mask=0x00
[ 1432.722549] ===>in ds901b964_work_func() need reset? YES!!!
[ 1432.742589] in mxc_ipu_channel_reset() start
[ 1433.382653] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1433.382697] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1433.382782] in mxc_ipu_channel_reset() end
[ 1433.410555] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1433.410575] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1433.410593] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1433.442608] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1433.483487] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1433.524391] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1433.557719] ===>in ds901b964_irq_handler() IRQ handler
[ 1433.568423] ===>in showTI964Status(): STS=0x92
[ 1433.568435] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x00 ST2[0]=0x02
[ 1433.568445] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1433.568453] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1433.568460] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1433.568466] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1433.568472] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1433.568477] in showTI964Status() # IS_RX1 DETECTED 
[ 1433.568482] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1433.568487] in showTI964Status() 0: # NO_FPD3_CLK DETECTED 
[ 1433.568493] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1433.568498] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1433.568504] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1433.568509] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1433.568516] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1433.568520] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1433.568525] in showTI964Status() 1: # PORT_PASS=1 
[ 1433.568530] in showTI964Status() 1: # LOCK_STS=1 
[ 1433.568535] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1433.568540] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1433.568544] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1433.568548] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1433.568553] in showTI964Status() 2: # PORT_PASS=1 
[ 1433.568557] in showTI964Status() 2: # LOCK_STS=1 
[ 1433.568561] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1433.568566] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1433.568570] in showTI964Status() 3: # PORT_PASS=1 
[ 1433.568574] in showTI964Status() 3: # LOCK_STS=1 
[ 1433.568578] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1433.568585] ds901b964_work_func old_mask=0x0E new_mask=0x0E sub_mask=0x00 add_mask=0x00
[ 1433.568590] ===>in ds901b964_work_func() need reset? YES!!!
[ 1433.583680] in mxc_ipu_channel_reset() start
[ 1434.192631] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1434.192667] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1434.192712] in mxc_ipu_channel_reset() end
[ 1434.228438] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1434.260462] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1434.301360] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1434.342248] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1434.424101] ===>in ds901b964_irq_handler() IRQ handler
[ 1434.435304] ===>in showTI964Status(): STS=0x91
[ 1434.435330] LO[0]=0x03 HI[0]=0x00 ST1[0]=0x13 ST2[0]=0x00
[ 1434.435340] LO[1]=0x60 HI[1]=0x00 ST1[1]=0x43 ST2[1]=0x45
[ 1434.435347] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1434.435355] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1434.435362] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1434.435368] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1434.435373] in showTI964Status() # IS_RX0 DETECTED 
[ 1434.435379] in showTI964Status() 0: # IS_PORT_PASS DETECTED 
[ 1434.435384] in showTI964Status() 0: # IS_LOCK_STS DETECTED 
[ 1434.435389] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1434.435394] in showTI964Status() 0: # LOCK_STS_CHG DETECTED 
[ 1434.435399] in showTI964Status() 0: # PORT_PASS=1 
[ 1434.435404] in showTI964Status() 0: # LOCK_STS=1 
[ 1434.435409] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1434.435414] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1434.435418] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1434.435423] in showTI964Status() 1: # PORT_PASS=1 
[ 1434.435427] in showTI964Status() 1: # LOCK_STS=1 
[ 1434.435431] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1434.435436] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1434.435440] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1434.435444] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1434.435449] in showTI964Status() 2: # PORT_PASS=1 
[ 1434.435453] in showTI964Status() 2: # LOCK_STS=1 
[ 1434.435457] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1434.435461] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1434.435466] in showTI964Status() 3: # PORT_PASS=1 
[ 1434.435470] in showTI964Status() 3: # LOCK_STS=1 
[ 1434.435474] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1434.435481] ds901b964_work_func old_mask=0x0E new_mask=0x0E sub_mask=0x00 add_mask=0x00
[ 1434.435486] ===>in ds901b964_work_func() need reset? YES!!!
[ 1434.454118] in mxc_ipu_channel_reset() start
[ 1434.678275] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001
[ 1434.852631] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1434.852672] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1434.852758] in mxc_ipu_channel_reset() end
[ 1434.852775] ===>in ds901b964_irq_handler() IRQ handler
[ 1434.863412] ===>in showTI964Status(): STS=0x91
[ 1434.863422] LO[0]=0x63 HI[0]=0x00 ST1[0]=0x13 ST2[0]=0x45
[ 1434.863431] LO[1]=0x00 HI[1]=0x00 ST1[1]=0x43 ST2[1]=0x04
[ 1434.863438] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1434.863445] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1434.863451] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1434.863457] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1434.863462] in showTI964Status() # IS_RX0 DETECTED 
[ 1434.863468] in showTI964Status() 0: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1434.863473] in showTI964Status() 0: # IS_LINE_CNT_CHG DETECTED 
[ 1434.863478] in showTI964Status() 0: # IS_PORT_PASS DETECTED 
[ 1434.863483] in showTI964Status() 0: # IS_LOCK_STS DETECTED 
[ 1434.863489] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1434.863495] in showTI964Status() 0: # LOCK_STS_CHG DETECTED 
[ 1434.863499] in showTI964Status() 0: # PORT_PASS=1 
[ 1434.863504] in showTI964Status() 0: # LOCK_STS=1 
[ 1434.863509] in showTI964Status() 0: # LINE_LEN_CHG 
[ 1434.863514] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1434.863553] in showTI964Status() 0: # LINE_CNT_CHG DETECTED 
[ 1434.863559] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1434.863564] in showTI964Status() 1: # PORT_PASS=1 
[ 1434.863568] in showTI964Status() 1: # LOCK_STS=1 
[ 1434.863572] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1434.863577] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1434.863581] in showTI964Status() 2: # PORT_PASS=1 
[ 1434.863585] in showTI964Status() 2: # LOCK_STS=1 
[ 1434.863589] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1434.863594] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1434.863598] in showTI964Status() 3: # PORT_PASS=1 
[ 1434.863602] in showTI964Status() 3: # LOCK_STS=1 
[ 1434.863606] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1434.863613] ds901b964_work_func old_mask=0x0E new_mask=0x0F sub_mask=0x00 add_mask=0x01
[ 1434.863618] ===>in ds901b964_work_func() need reset? YES!!!
[ 1434.882596] in mxc_ipu_channel_reset() start
[ 1434.882729] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1434.882749] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1434.882766] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1435.037616] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1435.037657] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1435.037734] in mxc_ipu_channel_reset() end
[ 1435.046295] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1435.046313] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1435.046328] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1435.078451] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1435.119365] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1435.160243] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1435.493632] ===>in ds901b964_irq_handler() IRQ handler
[ 1435.505141] ===>in showTI964Status(): STS=0x92
[ 1435.505160] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1435.505170] LO[1]=0x03 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x04
[ 1435.505178] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1435.505185] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1435.505190] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1435.505196] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1435.505202] in showTI964Status() # IS_RX1 DETECTED 
[ 1435.505208] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1435.505213] in showTI964Status() 0: # PORT_PASS=1 
[ 1435.505218] in showTI964Status() 0: # LOCK_STS=1 
[ 1435.505223] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1435.505227] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1435.505232] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1435.505237] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1435.505241] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1435.505245] in showTI964Status() 1: # PORT_PASS=1 
[ 1435.505250] in showTI964Status() 1: # LOCK_STS=1 
[ 1435.505254] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1435.505259] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1435.505263] in showTI964Status() 2: # PORT_PASS=1 
[ 1435.505267] in showTI964Status() 2: # LOCK_STS=1 
[ 1435.505271] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1435.505276] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1435.505280] in showTI964Status() 3: # PORT_PASS=1 
[ 1435.505284] in showTI964Status() 3: # LOCK_STS=1 
[ 1435.505288] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1435.505296] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1435.505300] ===>in ds901b964_work_func() need reset? YES!!!
[ 1435.522605] in mxc_ipu_channel_reset() start
[ 1435.662642] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1435.662686] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1435.662772] in mxc_ipu_channel_reset() end
[ 1435.700602] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001
[ 1435.700624] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1435.700641] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000002
[ 1435.732761] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1435.773682] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1435.814542] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1436.459110] ===>in ds901b964_irq_handler() IRQ handler
[ 1436.469838] ===>in showTI964Status(): STS=0x92
[ 1436.469850] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1436.469858] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1436.469866] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1436.469874] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1436.469881] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1436.469887] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1436.469892] in showTI964Status() # IS_RX1 DETECTED 
[ 1436.469898] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1436.469903] in showTI964Status() 0: # PORT_PASS=1 
[ 1436.469908] in showTI964Status() 0: # LOCK_STS=1 
[ 1436.469913] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1436.469919] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1436.469924] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1436.469929] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1436.469934] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1436.469940] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1436.469945] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1436.469949] in showTI964Status() 1: # PORT_PASS=1 
[ 1436.469953] in showTI964Status() 1: # LOCK_STS=1 
[ 1436.469959] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1436.469963] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1436.469968] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1436.469973] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1436.469978] in showTI964Status() 2: # PORT_PASS=1 
[ 1436.469984] in showTI964Status() 2: # LOCK_STS=1 
[ 1436.469989] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1436.469995] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1436.470000] in showTI964Status() 3: # PORT_PASS=1 
[ 1436.470004] in showTI964Status() 3: # LOCK_STS=1 
[ 1436.470008] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1436.470015] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1436.470020] ===>in ds901b964_work_func() need reset? YES!!!
[ 1436.482598] in mxc_ipu_channel_reset() start
[ 1436.602647] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1436.602686] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000003
[ 1436.602730] in mxc_ipu_channel_reset() end
[ 1436.641166] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000002
[ 1436.673342] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=1
[ 1436.714215] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=2
[ 1436.755114] in mxc_v4l_dqueue() back buffer, and return time out, pxd->frame_buffer=3
[ 1438.119259] ===>in ds901b964_irq_handler() IRQ handler
[ 1438.131004] ===>in showTI964Status(): STS=0x92
[ 1438.131018] LO[0]=0x00 HI[0]=0x00 ST1[0]=0x03 ST2[0]=0x04
[ 1438.131027] LO[1]=0x63 HI[1]=0x00 ST1[1]=0x53 ST2[1]=0x45
[ 1438.131034] LO[2]=0x00 HI[2]=0x00 ST1[2]=0x83 ST2[2]=0x04
[ 1438.131041] LO[3]=0x00 HI[3]=0x00 ST1[3]=0xc3 ST2[3]=0x04
[ 1438.131048] in showTI964Status() # GLOBAL INTERRUPT DETECTED 
[ 1438.131054] in showTI964Status() # IS_CSI_TX0 DETECTED 
[ 1438.131058] in showTI964Status() # IS_RX1 DETECTED 
[ 1438.131064] in showTI964Status() 0: # RX_PORT_NUM = RX0  
[ 1438.131070] in showTI964Status() 0: # PORT_PASS=1 
[ 1438.131074] in showTI964Status() 0: # LOCK_STS=1 
[ 1438.131079] in showTI964Status() 0: # FREQ_STABLE DETECTED 
[ 1438.131085] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED 
[ 1438.131090] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED 
[ 1438.131094] in showTI964Status() 1: # IS_PORT_PASS DETECTED 
[ 1438.131099] in showTI964Status() 1: # IS_LOCK_STS DETECTED 
[ 1438.131104] in showTI964Status() 1: # RX_PORT_NUM = RX1 
[ 1438.131109] in showTI964Status() 1: # LOCK_STS_CHG DETECTED 
[ 1438.131113] in showTI964Status() 1: # PORT_PASS=1 
[ 1438.131118] in showTI964Status() 1: # LOCK_STS=1 
[ 1438.131122] in showTI964Status() 1: # LINE_LEN_CHG 
[ 1438.131127] in showTI964Status() 1: # FREQ_STABLE DETECTED 
[ 1438.131131] in showTI964Status() 1: # LINE_CNT_CHG DETECTED 
[ 1438.131136] in showTI964Status() 2: # RX_PORT_NUM = RX2 
[ 1438.131140] in showTI964Status() 2: # PORT_PASS=1 
[ 1438.131144] in showTI964Status() 2: # LOCK_STS=1 
[ 1438.131148] in showTI964Status() 2: # FREQ_STABLE DETECTED 
[ 1438.131153] in showTI964Status() 3: # RX_PORT_NUM = RX3 
[ 1438.131157] in showTI964Status() 3: # PORT_PASS=1 
[ 1438.131161] in showTI964Status() 3: # LOCK_STS=1 
[ 1438.131199] in showTI964Status() 3: # FREQ_STABLE DETECTED 
[ 1438.131208] ds901b964_work_func old_mask=0x0F new_mask=0x0F sub_mask=0x00 add_mask=0x00
[ 1438.131214] ===>in ds901b964_work_func() need reset? YES!!!
[ 1438.142590] in mxc_ipu_channel_reset() start
[root@TSH-DEMO /home/root]# 

[ 1382.194945] in showTI964Status() 1: # IS_LINE_LEN_CHG INTERRUPT DETECTED
[ 1382.194949] in showTI964Status() 1: # IS_LINE_CNT_CHG DETECTED

Attached is their register setup. Could you help review about it? and give some solution。

DS90UB964 register.docx