Part Number: DS90UH948-Q1
Other Parts Discussed in Thread: DS90CF388A, TFP410, DS90UH949-Q1,
I am using this IC in conjunction with DS90CF388A and then TFP410 in order to build a FPD-Link III to HDMI converter (the reverse of this DS90UH949-Q1)
I am planing to configure DS90UH948-Q1 with "2-lane FPD-Link III Input, Single Link OpenLDI Output" but since the output can range between 50 and 192 MHz and the OpenLDI receiver I found only supports frequencies up to 112MHz I am a little bit lost since I don't find any other IC that better fits my design.
I don't know if I am getting this right. I can change all the ICs I am currently planing to use if I need to.