Hello,
I am planning on using the SN65LVDS150 to take in a 1.125Vpp, 10MHz sine wave into its +input, and biasing the –Input to Vt or a different voltage
The Common-mode Input voltage Vic limits are a little strange in the “recommended operating conditions”?
One table says 2.4-(Vid/2) =2.1V?, The Second table says Vcc-0.8V = 2.5V?
Which one is the correct MAX Common-mode Input voltage Vic limit?