This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: Is it possible to apply USB_VBUS pin up to 1.4V without VDD and VDD33?

Guru 29720 points
Part Number: TUSB4020BI


Hi Team,

Is it possible to apply USB_VBUS pin up to 1.4V without VDD and VDD33? (VDD and VDD33 are powered-off in this case.)
I would like to know if it could damage the device or not.
I believe it is possible however would like to confirm just in case.



Best Regards,
Yaita