Other Parts Discussed in Thread: ESDS302
Hi,
The recommended Input voltage range which is mentioned in ESDS312 data sheet is from 0V to 3.6V, so can ESDS312 be used as the surge and esd protection diodes for D+, D- and VBUS on USB 2.0 ?
Additionally, please tell me how to prevent latch-up when IEC 61000-4-2 Contact Discharge is applied continuously at +/- 8kV.
(e.g.: Adding other surge protection diodes)
Best regards,
Kato