Hi Team,
May I ask whether 941 can be compatible with 904?Because of cost, customer consider changing 926 to 904.
I know 941 is third, 904 is second is it backwards compatible?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
May I ask whether 941 can be compatible with 904?Because of cost, customer consider changing 926 to 904.
I know 941 is third, 904 is second is it backwards compatible?
Thanks!
Hi,
it is not recommended.
For UB904, this only supports pclk from 10MHz to 43MHz while ub941as's PCLK is from 25MHz to 210MHz. also ub904 only supports RGB666, maybe ub904 is not compatible in your system.
regards
Steven
Hi Steven,
Thanks for your quickly reply.
The pclk range and RGB666 can meet customer requirements.
In addition to pclk and RGB format, can 941 work together with 904?
I am not sure whether 904+941 works or not, because in 941's datasheet, only mention 941 worked with 92x....
Yes, Ameli.
UB941as is not validated with UB90x, so we don't suggest your customer to select UB904 paired with 941as.
best regards,
Steven