Hi
we are using TPD1E01B04 for ESD and surge protection of USB 3.0, USB 2.0, SATA ,Ethernet interface & Power line.
IEC 61000-4-5 Surge Protection – 2.5 A (8/20 µs) is the specification as per the datasheet of TPD1E01B04.
But as per the standard IEC 61000-4-5 currents are very high upto 2000A (source impedance=2 ohm) for power lines & 96A(source impedance=42 ohm) for signal lines.
I could not able to understand how i should this 2.5A with the standard values.
{we chosen this because of it has VBRF=6.4 V ,VRWM=+/–3.6 , low CL , high bandwidth and is recommended solution for above interfaces as per the ti ESD selection guide}
will this IC help me in passing TPD1E01B04 { IEC 61000-4-2,IEC 61000-4-4 and IEC 61000-4-5 } all are at high levels.IF no can you suggest me an alternate option in meeting listed standard.
thanks
Bhanu