This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933-Q1: AR0239AT RGB-IR format

Part Number: DS90UB933-Q1


Hi Sir 

May I know DS90UB933-Q1 can support RGB-IR format of AR0239AT?

Thanks

  • Hi Kai,

    The DS90UB933-Q1 transmits parallel data in 10 or 12 bits. As long as this imager can transmit parallel data with 10 or 12 bits, then it'll be fine. From the product overview, it seems like they have an output interface for parallel with Dout[11:0] +PCLK+LV+FV, so you can set-up the 933 for 12-bit mode and it should work. I would just double check with OnSemi to make sure there's no other requirement for Parallel output in this format form their end.

    Regards,
    Mandeep Singh