This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LV31E-EP: 1.8V Low-Voltage High-Speed Quadruple Differential Line Drivers

Part Number: AM26LV31E-EP
Other Parts Discussed in Thread: AM26LV31, SN65HVD01

Do you have a equivalent part for "AM26LV31" with 1.8V I/O support ?

  • Hi Shekhar,

    We unfortunately do not have such a device.  We do have a single transceiver with 1.8-V IO support in SN65HVD01; you could use four of those devices in a quad-channel application.  Besides that, another solution would be to simply pair the AM26LV31 with a 3.3-V/1.8-V level shifter.

    Regards,
    Max