This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

recommend alternative to SN65LVDT348 with 5V TTL output

Other Parts Discussed in Thread: SN65LVDS391, SN65LVDT348, DS90C402

Hello TI-Community,

i am searching for a LVDS Driver & Receiver Pair with this requirements:

  • single-way (Master to slave only)
  • 2x 2-wire SPI (clock + data) = Quad channel
  • low-speed Data Transfer Rate: max 35 MHz needed
  • >10..30 Meter twisted pair cable (Cat.5e)
  • driver:
    • 3.3V power and TTL logic input
  • receiver:
    • 5V power and TTL logic output
    • integrated termination resistor

what are the key aspects in the datasheets to look out for with this requirements?

for a 3.3V in and out system i have ready to test on my desk

  • Driver: SN65LVDS391
  • Receiver: SN65LVDT348

so i am searching for a good alternative to SN65LVDT348.
if i understand this correct the 348 has a high immunity against all sorts of
miss-alignment and noise from the environment and distance between devices..

but i have not found a similar 5V TTL compatible device - with this 'advanced' functions/parameters?!
maybe it is better /required to do a separate level-shifting at the receiver side?!

thanks for any hints or information how to find this :-)

sunny greetings
stefan