Hey
I have a system using TCA6416AZQSR, its a very small PCB so size is really matters
I see in the web that TCA6416AZQSR is EOL (End Of Life), is there any replacement?
BR
Elhanan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey
I have a system using TCA6416AZQSR, its a very small PCB so size is really matters
I see in the web that TCA6416AZQSR is EOL (End Of Life), is there any replacement?
BR
Elhanan
Hello Elhanan,
The most straightforward replacement would be the QFN version of the same device, which is unfortunately slightly larger at 4 mm x 4 mm. Do you think this would be an option for you?
Regards,
Max
Hello
QFN Version is to large for me.
can you tell me if your device was compatible to NXPs PCA6416AEVJ?
BR
Elhanan
Hello,
Yes, these devices should be compatible with one another. They have the same pinout and functionality.
Regards,
Max