Other Parts Discussed in Thread: SN65LVDS048A,
I am using the SN65LVDS047PWR to convert single-ended SPI signals to differential signals that can be sent along on cat5e cable. Each differential output is terminated with a 100-ohm resistor at the end, before being input into an SN65LVDS048A quad LVDS receiver. When I input a test clock signal (about 10kHz) into the inputs of the first and second drivers on the chip I get the expected differential outputs. When I input that same test clock into the third driver the differential outputs are fixed at roughly +2.6V relative to chip ground. The outputs do not change no matter what the input to the third driver is. I am powering the chip with +3.3V, and the input clock swings from 0-3.3V.
I have tried replacing the chip in the circuit, thinking that it might have been damaged by ESD or heat from soldering (even though it was reflowed with the correct profile) but the behavior of the third driver was unchanged between different chips.
Any help in diagnosing this would be greatly appreciated.
P.S. There seems to be an error in the SN65LVDS047 datasheet on the first page in the functional block diagram. The output of the AND gate shouldn't be tied to the input of the fourth driver, it should be tied to the enable line of the third driver.