Other Parts Discussed in Thread: SN65HVD233,
Experiencing similar issues, even with the ceramic part rated to 210C. Was a solution found?
Thank you,
Stephen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Experiencing similar issues, even with the ceramic part rated to 210C. Was a solution found?
Thank you,
Stephen
Hi Stephen,
I'm gathering information on the previous thread to see if we found a solution. I will give you an update later today based on what I find.
Regards,
Eric
Hi Stephen,
I was able to trace some internal communications regarding the previous E2E thread, but I was not able to find if the issue was resolved. Luckily the information I can access elaborates more on the testing that was done. Would you be able to provide more information on your testing so that we can see if this may be a similar occurrence?
1. At what time and temperature during the test does the failure occur?
2. In what way does the device fail? - If there is a communication failure, would you be able to share scope shots of the CAN bus being driven by the failed part?
3. How many devices have failed the test? - Are the failure results repeatable and if so at what rate?
4. Do other devices in the system fail as well? - Other ICs, traces, passive components, etc. Could any of this cause a transient or surge event?
5. What other devices are connected to SN65HVD233 during the test? - Is communication present during the test? Could you share a schematic?
6. Could you share the marking that are on the top of the failed device(s)?
Regards,
Eric
Hi Stephen,
Were you able to find a solution for the SN65HVD233-HT failure at high temp?
Regards,
Eric