Other Parts Discussed in Thread: TUSB8041
Will the board work if I design the circuit like the TUSB8041EVM without any additional firmware work?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will the board work if I design the circuit like the TUSB8041EVM without any additional firmware work?
Hello Hyunwoo Kim,
Yes, the TUSB8041 is designed to work without any EEPROM or SMBUS host required. Please note that if you will be configuring the hub using pin configuration only, do not install an EEPROM and remember to set SMBUSz = 1.
Regards,
JMMN
Thanks for the quick response.
Looking at the EVM schematic, there is a connector for JTAG,
Is this function not actually used?
Correct, the JTAG is only for internal test mode. The EVM design is also the lab evaluation board design so it has some unpopulated extra features that are not needed by end users.
Regards,
JMMN