This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: do we need to configure other things if 949's Dout1 connnected with 926 instead of Dout0 connected with 926?

Part Number: DS90UB949-Q1
Other Parts Discussed in Thread: ALP

Hi Team,

My customer now want to use 949's Dout1 to connect with 926 in instead of Dout0, because of some PCB layout error...

As my understanding, it could be automatic detection which lane contect to 926. 

But as customer's feedback, even they open the pass through, there is no link between 949 and 926.

When 949 connect with ALP, they can't detect 926.

So do we need to configure other things if 949's Dout1 connnected with 926 instead of Dout0 connected with 926?