This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867ERGZ-R-EVM: 1.8V power supply

Part Number: DP83867ERGZ-R-EVM

Hi,

  We use DP83867ERGZT ,the datasheet say

1.8-V Analog Supply (±5%).
No external supply is required for this pin. When unused, no connections
should be made to this pin.
For additional power savings, an external 1.8-V supply can be connected to
these pins. When using an external supply, each pin requires a 1-μF and 0.1-
μF capacitor to GND.

I want to know the meaning of  power saving . 1.8V pin  no connection or  external supply connect,witch way is Recommended