This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1208: Input voltage question

Part Number: LMH1208

Hi Team,

Would you advise Vin0_cm voltage question from my customer below?

■ Check item
I am trying to input LVDS to IN0 +/- of this device.
Looking at the data sheet below, the common mode voltage is high, which is typ 2.06V.

1. When DC coupled, does the input differential signal (LVDS) VCM (crosspoint) need to be around 2.06 V?

Or

2. In case of DC coupling, VCM (cross point) of input differential signal (LVDS) is in the range of 0 to 2.06 V.

Which is the recognition?

□ Composition
LVDS => LMH1208RTVT

□ LVDS specifications
VCM-OUT: typ 1.2 V
| VOD-Diff | = typ 300 mV

□ LMH1208RTVT specifications
VIN0_CM: typ 2.06 V
CD ON_IN0: typ 20 mV p-p

Thanks

Best regards,

Shidara