Hello,
We have an issue with using the TPS65987D as the source to power a device with a TPS65986. As you can see below, the negotiation jumps back to 5V from 12V and it's unclear why:
Here how it should look (see line 41)
How it looks once running:
As you can see at line 42 it jumps back to 5V.
In addition find a scope shot of CC1 at that moment:
These test are being done with a TPS65987EVM.
Do you know hat could be an issue?
Thank you and best regards,
Ambroise