Hi,
in our design we are planning to use TUSB1046-DCI mux switch it interface Dispaly port lines and USB-3 lines to the Type C connector. We are using DP and USB in Downstream mode only (DFP) and NO Power delivery, do we need a Typec-controller to interface with TUSB1046-DCI, If yes kindly suggest one from TI . Is there any option we can use it with out any controller? if yes then how we can get HPD lines and interface CC lines?