This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042HG-Q1: p2p compatibility with and without level shifters

Part Number: TCAN1042HG-Q1
Other Parts Discussed in Thread: TCAN1042V-Q1, TCAN1042-Q1

Hi All,

Currently my customer is using TCAN1042V-Q1 (TCAN1042HVDRBRQ1) with "V suffix"  that is with integrated level shifters.
He would like to replace on another board the SN65HVD251D / SO8 with the transceiver TCAN1042-Q1 but, having the first only the VCC (5V), I would need the version without level shifters (without V suffix, ie TCAN1042HGDRBTQ1) so that I can replace the second to the first without changes.

Can you please confirm that the variants with and without V have the same characteristics, as it seems from the datasheet?

Many Thanks,

Antonio