This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1208: IN0+/- Input Voltage

Part Number: LMH1208

Hi Team,

IN0+/- are required external 4.7uF, AC-coupling capacitors.
So IN0+ and IN0- swing centered around 0V.

On the other hand, input common voltage(VIN0_CM) is 2.06V(typ).

I guess IN0+/- have internal pull-up and pull-down resistance.

Ex.)5k_Ohm Pull-up and 8k_Ohm Pull-down for 2.03V

Is this guess correct?
Then, would you pls tell me internal resistance value?

Best regards,
Hasegawa