Hi Team
Just want to simplify the question.
When using 921/948, could customer use I2S_CLK to transfer PWM from 921 to 948? If yes, how to configure?
Thanks!
*******original *************
At present, in ti949->ti948, pwm signals can be transparently transmitted through gpio3, but because we have three screens, we use ti949, ti947, and ti921 respectively, but the gpio port of ti921 is occupied, only the I2S_CLK pin can be used, considering the hardware design For uniformity and future mass production, only the I2S_CLK pin can be used to transparently transmit the pwm signal, but there are some problems currently, so please give me some advice:
Set ti949 register: 0x12->0x0b 0x1a->0x09
Set ti948 register: 0x21->0x09
I now set my PWM to 1k and 1M, and it can’t be transmitted transparently, and the I2S_CLK of ti948 has a 3.072M clock.
Could you please give any advice about this?