I'm using TPD2E001DRL part in my schematics. In order to start Layout work i need the S-parameter model for this ESD.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Vipin,
Unfortunately, TPD2E001 is a fairly old part, and we do not currently have the s-parameter model for it. However, that part has a 1.5 pF capacitance, so it should work fine for relatively slow signals.
What is the application you are using this part for, and why do you need the s-parameter model? If you are using a higher speed signal, I can recommend another part for you.
Regards,
Matt Smith
This ESD is used for USD 2.0 signals at a data rate of 480Mbps.
The S-parameter model is for the simulation and validation of layout.