TVS1400DRVR is used on the power line of the power connector (hot plug).
When the power is turned on with the hot plug, the inrush current will increase if the TVS1400DRVR is used.(As much as with a 1uF capacitor)
When the TVS1400DRVR is removed, the inrush current becomes smaller.
The data sheet states that the TVS1400DRVR has a low capacity (120pF), so I thought it would not affect the inrush current, but it wasn't.
Can you see why the inrush current is so high when using the TVS1400DRVR?
Best regards,