Other Parts Discussed in Thread: AM5726
Hi Etherphy team,
I have a question about DP83869HM.
Question 1
Due to layout issue, there are reverse polarity connection between connector and phy.
Does DP83869HM supports reverse polarity connection?
Question 2
reverse polarity and normal polarity is mixed as below but is it ok to use below configuration?
A: reverse polarity
B: normal polaritry
C: reverse polarity
D: reverse polarity
Question 3
DP83869HM supports IEEE802.3.
If phy supports IEEE802.3, is it ok to say that phy also supports IEEE802.3x(flow control) or additioanl comment is needed like "phy supports IEEE802.3 and IEEE802.3x"?
Question 4
Have you heard any 10Base-Te negotiation trouble between DP83869HM and AM5726?
Regards,
Kai