Hi
is the EEPROM optional or must be used? If we don't use EEPROM, any limitation for the application? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
is the EEPROM optional or must be used? If we don't use EEPROM, any limitation for the application? Thanks.
Hi Wayne,
For TUSB8041-Q1 normal operation an EEPROM is optional as long as default USB descriptors can be used. If USB descriptors need to be changed then EEPROM is required.
HI Malik,
Thanks for your help.
I searched four key words of descriptors in the datasheet, in 8.5.5, such as device descriptors, do you mean the descriptors are these things?
Hi Wayne,
Most registers in Table 3. TUSB8041-Q1 Register Map will impact the USB Hub descriptors. See the full section 8.5 of datasheet for more details on these registers. Below is a list of examples where customer would need to implement a EEPROM. This list excludes features that can be configured through GPIO.