Part Number: SN65MLVD206B
Hi team,
My customer is evaluating SN65MLVD206B as backplane bus, they are finding a best choice for 150Mbps, so they tried many termination values.
However, when they use 43R as the two termination resistors value,(means 43R//43R = 21.5R equivalent differential impedance ), the V_AB is still 430mV, not 11.3mA*21.5 = 242.9mV.
Is SN65MLVD206B is a 11.3mA constant current output device as TIA/EIA-899 limit?
If yes, can you help comments why two 43R termination resistors in parallels leads to 21.5R equivalent impedance, but get 430mV not 11.3mA*21.5 = 242.9mV?
Thank you!
Best regards
Yunjing