Other Parts Discussed in Thread: SN74AUC2G66
Hi, Can VREF1 and VREF2 be same voltage? My customer would like to use 1.8V for both pins.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Can VREF1 and VREF2 be same voltage? My customer would like to use 1.8V for both pins.
Thanks!
No, this cannot be done. The recommended operation conditions table says:
(1) To support translation, VREF1 supports 1.2 V to VREF2 - 0.6 V. VREF2 must be between VREF1 + 0.6 V to 5.5 V.
This device is a passive switch and does not buffer the signals. If you want to disconnect the two sides, use an analog switch like the SN74AUC2G66.