Other Parts Discussed in Thread: SN65LVDS33
I am using SN65LVDS31 as a line driver and sn65lvds33 as a receiver. Both components are in the same module but on different Boards. There are 4 PCBAs in the module and driver is on 1st and Receiver is on the 4th PCBA. Total length of the Traces will be around 80 cm.
Both chips are supplied by same 3V3-DC-DC supply. I hope this is already a meant application for these two components.
For driver component, I add a pull down 4k7 resistor for open inputs and for related output I directly terminate it with 100 ohm at the output of the gate driver. Do you think is this the right approach?
Thank you for your help