This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1051H: May we know if TCAN1051HD can direct replace MAX13053A?

Part Number: TCAN1051H
Other Parts Discussed in Thread: TCAN1051

Hi Sir 

May we know if TCAN1051HD can direct replace MAX13053A?

I saw TCAN1051HD have FD function, is it a benefit? 

                                                  Bogey

  • Chen,

    The TCAN1051HD is the direct replacement for the MAX13053A, and they both have CAN FD capability with 2Mbps data rate. the TCAN1051HGD works up to 5Mbps, which would be a benefit over the MAX13053A. The common-mode range on the TCAN1051 family is better than MAX13053A as well. Otherwise, the devices are almost identical in terms of electrical parameters and function.

    Please let me know if you have any other questions.

    Regards,