Hi Sir
May i know what is TCAN1042HGVDR IEC1000-4-2 Air-Gap Discharge rating?
because our competitor have show but TCAN1042HGVDR i am not sure check which item.
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir
May i know what is TCAN1042HGVDR IEC1000-4-2 Air-Gap Discharge rating?
because our competitor have show but TCAN1042HGVDR i am not sure check which item.
Bogey
Chen,
As part of our certification testing, we don't perform IEC61000-4-2 air gap discharge testing, but we do air gap discharge based on the J2962-2 specification. This ESD testing is a derivative of the IEC61000-4-2 ESD test, but it uses a system approach rather than a singular device, and the RC network in the ESD striking tool is 2k ohms and 330pF, rather than 330 ohms and 150pF in the IEC61000-4-2 testing.
In the J2962-2 testing, our device survives to 15kV air discharge. Please let me know if this is helpful.
Regards,