This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: Does customer need to do any lab certification to make sure their product are CAN BUS compliant ?

Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550

Hi 

Does customer need to do any lab certification to make sure their product are CAN BUS compliant when using TCAN4550 ?

  • Hi,

    The integrated transceiver in TCAN4550 meets all of the requirements of the ISO 11898-2 CAN physical layer standard and is compatible with any CAN network that follows the same. As long as the end-system network is not too dissimilar to typical CAN topologies (system is properly terminated, has short stubs, and does not present excess capacitive or resistive loads), then there should be no problem integrating TCAN4550 into CAN systems.

    Let me know if you have any more questions.

    Regards,
    Eric Schott