Hi there,
I'm looking to design and build a 4:1 SDI input mux for a university project. From research the LMH0356 looks to be my best option for this, however, I'm fairly new to electronics, and so I'd like to build this circuit on a prototyping board or something similar, and so would need a socket for this IC. Is there such a thing as a socket for the WQFN 48 pin IC? And if there is how would I go about acquiring it? I'd be looking to build a circuit similar to the SD356EVK which is the evaluation board for this IC, as this would be my first choice of option however they're a bit out of my budget for a university project!
Thanks for your help!
Best regards,
Kieran