Other Parts Discussed in Thread: SN65HVD233
Hi,
we would like to use your SN65HVD230D in the following manner.
Mode 1 - normal can bus mode:
of course SN65HVD230D is ok.
Mode 2 - Can bus transmission disabled:
on the BUS there will be a 24 Vac or 24 Vdc ON/OFF signal managed by a photomos placed in parallel with the CAN bus.
Can we use SN65HVD230D or is better to move to an another device with an higher fault protection?
Best Regards,
Carloalberto Torghele