This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P82B96: Compatibilty

Part Number: P82B96
Other Parts Discussed in Thread: TCA9406, TXS0102,

Hi,

I would like to check on compatibility of this part (P82B96) for my application and if there are better options I should consider from TI.   I would like to run about 12 to 18 inch cable between boards and drive Ethernet MIIM signals(MDIO/MDC) MDIO/MDC @ 2Mbps if possible.  It is not clear if this product can run down to this rate as I did not see the relevant specification in the data sheet.  .Also will the TCA9406 or TXS0102 be better for this application, if so can you explain why and any specifics about configuration to consider.  

Thank you,

HSG